This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
I am making a constant current source using OPA353.My circuit is given below.
The frequency respose plot obtaned is also shown.
May I know is this respose expected.How to find the bandwidth of the complete circuit.
Regards
HARI
Hi Hari,
looks like you violate the common mode input voltage range of OPAmp. Set the DC input voltage different from zero Volt. Try 1V.
Can you post the TSC-file?
Kai
Hi Hari,
as I said the simu works with a DC input voltage of 1V:
Though, from the peak in the frequency response and the overshot in the transient analysis it can be seen that the circuit is not very stable.
Do you want support in increasing the stability of this circuit?
Kai
Hey Hari,
Have you seen this circuit?
Feedback components R3, R4, and C1 provide compensation to ensure stability. R3 isolates the input capacitance of the bipolar junction transistor (BJT), R4 provides a DC feedback path directly at the currentsetting resistor (R5), and C1 provides a high-frequency feedback path that bypasses the BJT.
All the best,
Carolina
Hi Hari,
I tried to compensate the circuit as discussed in the link given by Caro. But because the OPA353 is so fast I was not able to find a proper phase lead compensation for this circuit.
Do you really need to take the OPA353 in this circuit? What bandwidth do you need? And what is the load?
It seems that the chosen OPAmp and NPN do not fit well together. Can you take another NPN?
Please tell more about the application.
Kai
Hi Hari,
The load is our ASIC.
Do you know the load resistance? Is it a pure resistive load? Or is there any load capacitance and/or inductance?
And I would like to know why you need an aditional NPN output stage. I ask because the OPA353 has a rather strong output stage and can sink and source up to 40mA.
Kai
Hi Kai,
Regarding load resistance ,I will check with ASIC design team and let you know by tomorrow.
They will be flashing some fuses inside the ASIC.During that time ASIC will take 100mA of current.
Regards
HARI