Hello, the OPA207 may work with a single supply from 0 to +15 Vdc?
Thank you.
Regards
Paolo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, the OPA207 may work with a single supply from 0 to +15 Vdc?
Thank you.
Regards
Paolo
Yes, any single supply between 4.5 V and 36 V is supported.
Hi Paolo,
but keep an eye on the limited common mode input voltage range: Your input signal must stay 1.25V away from the supply rails. This might be a problem in a single supplied circuit.
Kai
Thank you Kai & Clemens,
Hi Paolo,
Yes the OPA207 supports a voltage supply from 4.5V to 36V, or ±2.25V to ±18V, but as Kai has mentioned, the input common-mode linear range requires 1.25V headroom away from the positive and negative supply. Please keep in mind the input common-mode range if using unipolar supply.
Thank you and Regards,
Luis