Part Number: INA239
The system routed "INA239" to the Amplifiers forum. Since it's actually a power (current/voltage) monitoring sensor, apologies if that's not correct forum.
The TI items are:
Sensor Control Board SENS077
Evaluation Module SENS064-002, INA239EVM
I am unable to get the link working between SCB and EVM. Hangup appears to be the firmware update.
Drivers were downloaded from link in manual: www.ti.com/.../sbac253. Downloads sbac253a.zip.
The PC OS is Win 10 Pro 22H2 (64 bit). The GUI & browsers tried are:
dev.ti.com/.../
Firefox 110.0 (64-bit)
Chrome Version 110.0.5481.104 (Official Build) (64-bit)
Have tried both USB ports on laptop, using USB cable supplied w/ evaluation kit.
TIA Cloud Agent (tiacloudagent_2) and the respective browser extensions installed through the GUI prompts on 1st access (only installed Cloud Agent once).
The 2 green lights on SCB and power light on EVM come on when plugged in to USB port. Driver creates COM 4 115200 port.
Then, along with "Firmware Update needed" popup, black box appears above the bottom GUI status bar w/ message:
Connected to SCB Controller, but failed to connect to SCB w/ INA239EVM, FW: v0.0.1.0 on DEFAULT
Have been able to get the Program Device menu item active. Clicking Program Device shows a Firmware Updating message, shows the circling-dot chaser, the green and red lights flanking the main chip on SCB flash once, then GUI says Flash failed. The GUI also loses contact with the SCB, although its power light is still lit.
I have also been able to get the green light to go off on the SCB by shorting the DFU test points + press reset. However, trying to update after that has same fail results.
The manual also mentions “Send the command 'bsl' on the SCB's USB Serial (COM) port.”. The GUI Scripting Window didn’t produce anything, so I tried TeraTerm on the COM port. I couldn’t get it into an interactive command mode, so was unable to try that.
The GUI log file of an attempt is attached.
Thanks
Steve