This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm using the LP339 in a motor control application to sense BEMF voltage levels and detect zero crossings. The inputs could see large common mode voltages. Vicr is recommend for 0V to Vcc-2. What happens above that recommended Vicr limit? Do I risk damaging the device or just an indeterminate output?
In my design Vcc = 12V and the common mode voltages could go to 15V.
Thanks for any guidance!
-Matt
Matthew,
The inputs can tolerate -0.3 to 30V (36 abs max). As long as one input is in the recommended voltage range then the output will be the correct state.
Below -0.3V would require a current limiting resistor and the output may be in the wrong state.
Regards,
Ron Michallick
Ravi,
The resistor prevents damage. The resistor won't prevent a temporary malfunction in the output.
It take only a little input current to get an output malfunction.