This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
Good day
As an example, suppose i want to use the 4 comparators on an LP339, in tina simulation. How do i change pins designation for U1, U2, U3 and U4 using the model without affecting spice netlist, etc ?
In other words, i d like Tina to figure out that LP339 is a quad, so that U1 would use: pin 2 as out, pin4 In-, Pin5 in+, than U2 is ``out`` to pin1, in- is pin6 , in+ pin7 and so on.
Any way to do this ?
Many tanks
JP