Hi
What is the current rating of the protection diodes on the INA238 IN+ and IN- pins?
I want to make sure there is no damage to the IC for negative voltages.
The datasheet specifies that the maximum "Input current into any pin" is 5 mA. Can I use this as the rating, or is there a better figure available?
regards
Heiko