Other Parts Discussed in Thread: THS3201
Hello,
I am currently working on a characterization board with several THS3201, configured in simple voltage follower, inverter or gain of 2 or 3.
Several devices seem to be failing, as I experience on some devices offset higher than 100 mV and huge noise (more than 100 mV p-p), with increase in power consumption as well (up to 100 mA), when the input is grounded, although they still amplify signals when there is any. For some devices, these symptoms only appear a few minutes after power cycling.
The output of the devices feed an analog mux.
I would like to know is there are some likely/classical causes that could explain this specific type of failure... or not (?).
Thanks