This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS3201: ths3201

Part Number: THS3201
Other Parts Discussed in Thread: THS3491, ,

Do I have to use decoupling capacitors in the DC bias circuit of this OpAmp?

  • Hi Mahsa,

    We always recommend decoupling capacitors in circuits as they have multiple benefits. On top of supplying current during transients, they also filter out noise coming from your power source. Power supply noise can be seen at the output of a device that does not have proper decoupling. In some cases, we have seen it can even result in oscillations. I would like to add that the THS3201 is not recommended for new designs, and we suggest looking into the THS3491 as a potential replacement.

    Best Regards,

    Ignacio

  • Hi Ignacio,
    Thanks for your reply. Do you have any suggestions for value of decoupling capacitors?
    Thanks for mentioning that. could you please let me know what is the reason that you do not recommend this opamp? would it have a very catastrophic effect?

    Regards,
    Mahsa


  • Hi Mahsa,

    Figure 65 in the THS3201 highlights our EVM schematic for this device and shows the decoupling capacitors used. Figure 3 in the THS3491EVM user's guide highlights the values used for that design. The user's guide can be found here. The reason it is not recommended is because there is a chance we will stop supporting the device. We are still in production for existing customers, but for new designs and continued long-term support we do not recommend implementing the THS3201.

    Best Regards,

    Ignacio

  • Dear Ignacio,
    Thanks for your reply.

    As I am using it for research, and we have already some THS3201s available, I will go for it at this stage.
    Btw, do you mean figure 56 or 65? 

  • Hi Mahsa,

    I was referencing Figure 65 as this highlights what was designed for the THS3201EVM however Figure 56 highlights the same idea.

    Best Regards,

    Ignacio