Part Number: THS3201
Other Parts Discussed in Thread: THS3491, , LMH6703
Dear TI team,
I intended to use TH3201 in my design, but just recently I noticed that you do not recommend using it for new designs and it is recommended to use THS3491 instead which is not proper for my application due to its lower bandwidth (900MHz BW compared with the previous 1.8GHz Bandwidth).
Moreover, low system delay is crucial in my design, which despite to higher slew rate, has more rise and fall time of THS3491 (1.3ns compared to 0.7/0.9ns) that imposes another problem for me.
In this regard, I would appreciate it if you could introduce me another alternative for THS3201 with a bandwidth of more than 1.5 GHz and a rise and fall time of less than 0.7ns.