Hi
I am using LM2904 IC as Non inverting opamp to increase the range. Op amp input voltage range is 1.44V to 2V and output should vary from 0 to 3.2 V to supply to micro. The Vdd of the opamp is 5V. How to select the resistor values for the non-inverting configuration. And please suggest RC filter values for the input and output(( because 10 percent of 50hz ripple is there in input)