Part Number: OPA810
Other Parts Discussed in Thread: TPS65133,
Q1:
Is there any requirement for selection power supply for this OP?
such as accuracy 5% or 1%, PSRR? load regulation?
Q2:
If use +/5V for this OP, should I use power supply like TPS65133?
Or should I use two seprate power supply, such 5V LDO for OP + ADC, and another -5V DC/DC for OP only?
Q3:
I would like to if it's necessary to use DC/DC to generate -6V, and then add LDO for -5V to have better peformance.