I've designed an instrumentation amplifier based on the 3 operational amplifiers topology as the following below. In the design, two op amps are implemented using TLV9352IDR and the third one is implemented with TLV9351QDBVRQ1. Both devices are supplied from +12V to -12V.
In this case, the input sense I have to sense is a differential voltage up to +/-48 Vdc and provide a proportional output up to +/-10Vdc. Sense voltage is made across R2 from input resistor divider R1-R2. When input is +/-48Vdc, R2 voltage is +/-3.3V and with the gain configured to 3, the output should be +/-10Vdc.
When input supply is positive, the instrumentation amplifier works correctly in the prototype. I've tried with input voltages of 5, 10, 24 and 48Vdc and output voltage results 1V, 2V, 5V and 10Vdc respectively.
However, when input voltage is negative, the instrumentation amplifier only works for low input voltages. I've tried with input voltages of 5, 10, 24 and 48Vdc and output voltage results -1V, -2V, -2.3V and -4.7Vdc, respectively.
Please, could you clarify me what is happening in the design? Have TLV9352IDR and TLV9351QDBVRQ1 an input voltage limitation or clamping?
Thanks in advance.