This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5424CQ1DKEEVM: Connecting Multiple Amplifier Evaluation Module Boards to a PC

Part Number: TAS5424CQ1DKEEVM

I bought four TAS5424CQ1DKEEVM evaluation boards and I connected all of them to the same PC using their USB-to-I2C boards.

I use the TAS54x4C EVM GUI, SLOC287, to control the amplifiers.

However, I can only see one of them at each time, and not control all of them.

Is there a way to connect all of them to a PC and controlling them simultaneously using the TAS54x4C EVM GUI?

Thanks!!

  • Hi Gal

       I'm sorry that the GUI is not designed in that way.

       There's maybe an option, that only use PC to control one board, and using flying wire to connect the I2C Bus from four boards together. In that way, the four boards could get the I2C at the same time and config together. But it's not fully guaranteed.