Other Parts Discussed in Thread: AMC3330
Dear Experts,
I am trying to use 3 no.s of AMC1350 to measure 3 phase voltage. Page 33 of data sheet shows a typical example to measure the 3 phase voltage, which is similar to my area of interest. I have a couple of doubts in this. I find the all three voltages are being measured wrt the neutral. Can the voltages can be measured across a unit of the resistor which is middle of the series network of a phase? In this case, the INN pin and GND1 pin cant be shorted because the signal would be a differential signal.
Next, the application illustrated in the datasheet is perfectly balanced. If the voltages are unbalanced, neutral voltage cannot be zero. so, the neutral cannot be connected to gnd, which is common for all the three ICs as shown in the figure. In that case, I doubt if that configuration works.
Regards,
Rajesh BN.