Part Number: VCA822
I want to design programmable gain block with VCA822. The IC has 100V/V gain range but at simulation, the recommended resistor values for 100V/V (Rf = 845 ohm, Rg = 16.9 ohm) do not provide 100V/V at VG = 1V. The result has big offset. However recommended resistor values for 10V/V ((Rf = 1000 ohm, Rg = 200 ohm) provide 10V/V at VG = 1V. Why is there so much difference these gain configurations?