Other Parts Discussed in Thread: LM324,
Hello,
The datasheet indicates that input voltage can be within -0.3V to +40V, without relation to VCC power supply.
Can you please confirm that :
- the device will not damaged by an input voltage on the IN+/- inputs when it is not powered (VCC=0V) ?
- if a voltage is present on the input before a voltage is applied on power supply, the part will start and run without problem
Thank you
Aurelien