Other Parts Discussed in Thread: LM2904LV, TLV9151-Q1
How to caculate the Vcm, in dual and single power supply cases?
What will happen if the Vcm over spec and why?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How to caculate the Vcm, in dual and single power supply cases?
What will happen if the Vcm over spec and why?

The guaranteed minimum upper limit of the input common-mode voltage range always is 2 V below the positive supply rail.
When the input voltage goes higher, the electrical characteristics will degrade, or the amplifier no longer work correctly. See section 2.2 of the Application Design Guidelines for LM324 and LM358 Devices.
In below application, if V+=5V, V-=0, what the Vcm is?
And , is any risk to damage the OP?

Hey Guozhu,
Is this a low or high side current sense?
Additionally, if you are looking at using a 5V supply, LM2904LV is created specifically for low-voltage (5.5V supply and below). It still has a similar common-mode limitation, but is resilient to phase reversal.
Best,
Jerry
hello, Jerry;
Yes, it is a high side current sense circuit.
In our design, the power supply of the OP is range from 5 to 6.5V, so maybe LM2904LV is not the suitable one. And it has Vcm limitation too.
The phase reversal here means if the inputs below the Vcm limitation, the outoup will react VOH or VOL correctly, but if it's higher than the Vcm limitation, the output will reverse?
if LM2904BQPWRQ1 input higher than the Vcm, what will happen? and it will damage the OP or not?

Phase reversal is a specific error mode that happens only for negative inputs. But when the inputs are above 3 V (for a 5 V supply), the amplifier will just not work correctly. (This does not damage it.)
To handle larger input voltages, you need an amplifer whose Vcm includes the positive rail, or with rail-to-rail inputs, like the TLV9151-Q1.