This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1200-Q1: AMC1200 -Q1

Part Number: AMC1200-Q1
Other Parts Discussed in Thread: AMC1200, AMC3301, AMC1300

Dear support,

I use AMC1200 to do current sensing in my design.

The input power of my design is DC 48V to 160V.

VDD1 & VDD2 = 5V, magnitude of current to measured =0.68A

But when i power up my circuit with 48V input, Rshunt= 350m Ohm burn.

1.Is it the current flow through the Rshunt too high?

  So i should add R93, R95, R86 & R90 resistor to limit the current flow through the Rshunt .

2.Please help to confirm my circuit design is correct or not?

  I refer to below schematic for my design.

Here i attached my schematic for your reference.

SCH-1096-00_Current Sensing.pdf

Thank you.

Regards,

Ku