Part Number: AMC1200-Q1
Other Parts Discussed in Thread: AMC1200, AMC3301, AMC1200EVM
Hi,
I use AMC1200 to do current sensing in my design below,

The reference circuit i use was based on below isolated amplifier current sensing tables.

However even the input voltage is different (50Vdc or 60Vdc, i always get the same output level for VoutP or VoutN.
VDD1 & VDD2 both supply with 5V.
| Vin (V) | VINP(V) | VINN(V) | VOUTP(V) | VOUTN(V) |
| 50 | 5.7 | 5.7 | 2.48 | 2.478 |
| 60 | 5.657 | 5.663 | 2.496 | 2.48 |
I upload my schematic design for your reference.
Please help to confirm my design is it mistake in schematic?
Why the output remains unchange even input power change?
Thank you.
Best regards,
Ku