Hello,
If I use the single power supply of TLV3603 with 30mV hysteresis, it could work normally, but if I used +-2.5V power supply, input is +-2V sine, and reference is GND, the output is always high.
TLV3603 is rail to rail input and output, so the input meet the input voltage range, I wonder why its output is abnormal when using dual power supply.
Best regards
kailyn