Other Parts Discussed in Thread: LM2903B, LM339LV, TL331LV, LM393LV, LM393
Hi Team,
We need a library file for TL391LV. I see a different model is available in the product page.
In folder i see LM2903B. Is it same for Tl391LV?
Thanks
Murugesan A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Clemens,
The library you are referring LM393LV for TL391LV is having so many subcircuit. i am using the fisrt one in that.
When i am running in Microcap simulator, it is taking to much time to get the graphs. But if i use older comparator TS391 it is taking less time to get the graphs.
Can you help me to run transient response at faster.
Thanks & Regards
Murugesan A
Hi Clemens,
With LM393_TI is running faster. But this is different architecture you referred in the earlier chat. Can you confirm whether the LM393LV library is correct.
Thanks
I do not know Microcap, but I've heard that it is slow. The LM393LV model appears to be more detailed.
Hi,
True, Can you please provide us the exact library with out additional detailed.
I have tried to shirnk the library i am facing the error statement like below,
...
Thanks
Hi Murugesan,
Sorry I am not familiar with Microcap but essentially all the subcircuits are needed as they were the building blocks and functions used in the top layer or top main circuit of the model.
For your issue, there needs to be an "ENDS." at the end of each subcircuit block.
We do have PSpice and TINA which you can use as these models are much more optimized to be used with these simulators.
Hi Chi Nguyen,
I am using the library downloaded from the site, and ".ENDS" are available for all the SUBCKT model in the library, Even through it takes more time.
And i am not sure about pspice model. i didn't used it.
Hi Murugesan,
Sounds good, sorry we couldnt help you further with Microcap. PSpice and TINA are available for download if you wish to use.