Part Number: INA317
Other Parts Discussed in Thread: INA326
Hi,
We are using INA317 in our design in which we are facing some problem.
We are giving 0.549 and 0.428 at the input and the gain is set to 10. So in this case the output should be 1.21V but the output is getting clamped to 1V. When we checked the datasheet we came across a common mode voltage vs output voltage graph.
I want to check with you that this issue we are facing is because of common mode voltage?
If that's the problem then can you please suggest pin to pin compatible IC which doesn't have the behavior like INA317 common mode voltage Vs output voltage graph?