Other Parts Discussed in Thread: TLV9304, INA149
Hello Dear TI,
We are building a 50Hz-6th order notch filter around TLV9302. We have used Filter Design Tool to setup the design parameters. I selected an 6th Bessel with following parameters:
- Order: 6
- Ao: 1.000 V/V
- Fc: 50 Hz
- BWp: 30 Hz
- Rp: 0.01000 dB
- BWs: 3 Hz
- Asb: -40.00 dB
After getting resistors vales we build our board (see picture for routing).
First results of prototype are big surprise. We have only -22dB at 50Hz. We are expecting much more ~-35db. Can you help with this topic?