Part Number: LMP7721
Other Parts Discussed in Thread: INA128, INA226, TINA-TI
Hello everyone! I have a big problem regarding my schematics...
To begin, I am trying to create a circuit that helps me measure the current on a Schottky diode that is polarized from 0.2 to 2.5V in 0.05V steps. The range of the current values is aprox. 1nA to 100mA. I've divided this range in 3 smaller ones, and tried to find a circuit to use for each one:
1. 1nA to 1uA - I chose the LMP7721, and I tried to configure it in TIA mode so that I can connect its output to an ADC and then to a MCU, but the problem seems to be that for my values, it returns negative voltages - I am not really sure how to work around this.

Something like that, after some corrections that I've got from another forum since I initially connected V- to GND......
2. 1uA to 1mA using INA128 - here I chose a Rg for a gain of 20, but then again, after the corrections regarding V- connection I realised that the values are also negative.

3. 1mA to 100mA - Using INA226 - didnt get to test this one, I've added a 0.75Ohm sense resistor for it, and it looks like this:

The first range using LMP7721 is the most important to the circuit.. can you help me find a solution regarding the configuration of this TIA in order to get some good values on the output?
PS: I know I am not good at designing circuits and those may have some mistakes, but I just need help here, because I don't know what to do about it.