This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA232: can not readout small current

Part Number: INA232

System at IDLE mode,bus voltage is 14V,current is around 0.8mA,when do SW readout,power is 0.0128W,Bus voltage is 14.016V,but current is 0A,please find details as below picture,

We did an experiment, adjusting the loading slowly to find out when we can read out non-zero current,and get below result,it seems the min. readout value is 0x0600 equals 1.3mA.Why it can not recognize 1LSB?

BTW,only 1pcs TPS563200DDC is used in this system,should be no harmonics of 500K.