Other Parts Discussed in Thread: UCC27424
Hello TI,
I am currently simulating the behaviour of INA381-Q1 during over current condition as shown in the below circuit. I have created an over current situation by placing a low resistance of 50 ohm across 28V which is connected to drain of the N-channel mosfet. Initially i have operated the device in 'transperant mode' by keeping the RESET pin low and observed expected behaviour from ALERT signal. Then during the over current condition, after 600us I made RESET high to keep the device in Latch mode. However, the ALERT signal didnt immediately go low instead It has oscillated for 25us before staying permanently low. Do you know why this 'oscillating' behavior occurs ? also I have disconnected ALERT signal from ENBA of mosfet driver(UCC27424) then the ALERT signal became low immediately without oscillations. Could you please look into this and advise the reason for this behavior ?
Best Regards,
Manoj.