Other Parts Discussed in Thread: ADS1115
Tool/software:
Hi,
I am designing a photodiode amplifier circuit by referencing to this document.
This is my schematic.
(I set the V_OFFSET to 0.1V using resistor.)
I prevented light from entering the photodiode to measure the dark current of the photodiode in this circuit.
When I set feedback resistor(R1) to 3.2Mohm, VOUT is about 200mV.
When I set feedback resistor(R1) to 1Mohm, VOUT is about 700mV.
I expected the VOUT to be output as (Ipd x R1) + V_OFFSET in my circuit.
But, when i changed feedback resister(R1) from 3.2M ohm to 1M ohm, VOUT inceased about 500mV.
I was wondering why the VOUT increased even though I lowered the feedback resistor.
Is there something wrong with my circuit?
Regards,
Youngjun.