Tool/software:
I'm currently designing a photodiode array circuit w/ 18 VEMD2023SLX01 (https://www.vishay.com/docs/83493/vemd2023slx01.pdf) photodiode components. Given limited pcb real estate and i/o pins, im interested in using the LMH32404 to easily amplify and multiplex data to downstream ADCs. I wanted to make sure that these are compatible with the photodiodes I'm working with (when applied with a 5V reverse voltage the datasheet indicates that the PD capacitance is 1.3pF and max current is 14uA, which makes me think at first glance it should be okay). Secondly, is it possible to use convert the outputs to single-ended rather than differential? Generally also interested in using ADCs on Arduino's, which do not accept differential inputs.