This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV1702: window comparison circuit design with TLV1702

Part Number: TLV1702
Other Parts Discussed in Thread: TLV1872, TLV1822

Tool/software:

Hi Team

Customer wanna design a window comparation circuit to sense the power voltage. it is VCC and -VCC, +15V and -15V. the threshold point is +12V and -12V.

is the TLV072 can be used as this design? if TLV1702 can works normal if the differential voltage between VCC and GND  keeps within 30V?