Part Number: BUF634A
Other Parts Discussed in Thread: BUF634
Tool/software:
Greetings,
I am testing BUF634AIDR as a replacement/upgrade for the obsolete OPA633KPG4. I currently have a prototype SMT-to-TH adapter board built: BUF634AIDR, 0.1uF caps on rails, and 10ohm resistor on BW adjust, TH pins to interface with legacy design CCA. I am seeing two issues, one of which I believe I know how to resolve, the other is this: there is an incredibly long time delay between power on and getting an output from the chip, approaching ~1min. I suspect there is a power issue, but I have not been able to determine the root cause..
The existing/legacy CCA (footprint for OPA 633) has +/-12V on the rails (within spec), and there two 0.1uF caps at the pins for the OPA633. The first step I did was increase the those caps to 10uF, however the chip showed now change. At this point, I am not sure how to proceed.
Any input is greatly appreciated.
Thank you