Part Number: LM393
Other Parts Discussed in Thread: TLV1812, TLV1822, LM339
Tool/software:
AB/BA interchange has been done. This time, 100% of the newly purchased batches are abnormal. The outputs of the old batches and the ON brand's LM393 are normal.
Application Circuit: Build a comparator circuit as shown in the following figure using LM393 to achieve overcurrent protection. Set a 6V reference voltage at the inverting input terminal, and connect the current detection at the non-inverting input terminal. The output terminal is pulled up to a 12V power supply through a 1k resistor, and a diode 1N4148 is used to feed the output voltage back to the non-inverting terminal to realize the overcurrent protection lockout function.

Raw material model and test waveform:


Note: Channel 4 is the output; Channel 3 is the inverting terminal; Channel 2 is the non-inverting terminal
Current material model and test waveform:


Note: Channel 4 is the output; Channel 3 is the inverting terminal; Channel 2 is the non-inverting terminal