This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
We want to use INA253 for current sensing, could you pls support to calculate if it can meet our accuracy requirement? thank you.
Irms : 3.0A
ADC resolution : 12 bit
Vref_ADC : 5.0V
Customer required accuracy : 2%
Hi,
The INA253 specification is able to guarantee 0.6% accuracy at room temperature for 3A.
To meet the resolution requirement, filtering is necessary that is 20kHz or lower. Additional error budget should be allocated to ADC itself.
Regards,
Guang
could you pls share the HW schematic for your proposal?
and do you have the special calculation tool for High temperature ?
Hi,
To limit bandwidth, the HW solution can be a simple RC filter at the output. For example, 300ohm + 50nF yields ~10kHz.
We don’t have a special tool for high temp. I did a rough manual calculation for 125˚C, the expected error is about 1.3%. In the future, once the use condition is specified, it will be possible to do a more accurate estimate, but I don’t expect the number to change too much.
Regards,
Guang