Tool/software:
Dear TI engineers:
I designed an amplifier circuit with LMH6626, the schematic diagram is shown below.
The theoretical gain should be 100 times, but in the actual test the gain is only about 12 times, which is so far off that I am confused
Inout voltage = 10mV(50 Ohm),Output voltage = 114mV
How can I modify the circuit to achieve 100x gain?
Thanks
Zhong Jun