Part Number: OPA192
Other Parts Discussed in Thread: LM2664, LM7705, TLV387
Tool/software:
Hi.
I have a problem with the OPA192.

OPA192 is used as a low impedance buffer to the input of the MCP2024 ADC.
From time to time, all of a sudden the OPA192 is defect.. The -5V is drawn down til almost ground and the current consumption goes to some 400mA.
I have been changing The OPA192 4 times now, and need an answer to WHY..
The first to OPA192 was blown with a different chargepump; The LM2664. So probably its not the cgarge pump itself.
Is there anybody with any clue to why this is happening?