Other Parts Discussed in Thread: XTR116,
Tool/software:
I have a circuit using an INA828 as the front end amplfier to a loadcell and the output 4-20mA current loop driver implemented using an XTR116.

I am very happy with the performance except for one attribute which is surprising given the INA828 is a differential input.
If I touch the loadcell body or the metal plate it is mounted on, the output of the XTR116 changes by 40mV across a 50ohm load so 0.8mA.
Given that bridge input goes into a purely differential input, how is a positive signal being generated?
The bridge impedance is 350ohm so quite low impedance.
Any recommendations?