Part Number: OPA2227
Other Parts Discussed in Thread: OPA2277, OPA186, OPA277, OPA188, OPA325
Tool/software:
Hi, professors.
I'm using OPA2227 (OPAx227 series) at single power supply condition. The supply voltage is about +5V to 0V.
Recently, I noticed the output seems unsteady when the power supply voltage is below +5V (e.g., +4.9V) than when I use above 5V (e.g., +5.1V).
Our circuit is a typical differential amplifier using two opamps included in the same package and some high precision resisters.
The measuring parameter is zero drift characteristics, and the input is biased about +2.5V by the same value resistors, and two amp's +input is shorted.
Temperature condition is +25℃ (const.) using a chamber.
I think different parameter is just the supply voltage.
Actually, under investigation, output is very clear and almost no drift when using +5.1V power supply.
Do you know the reason of this problem or the true recommended operating conditions?
I thought I should use over +5V power supply on OPAx227 series.
Best regards,