This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello Team,
I am exploring to use INA826 in unity gain configuration for industrial +/10V input stage design with ADS8688 bipolar input ADC. I checked one of the reference design https://www.ti.com/lit/ug/tidu491/tidu491.pdf?ts=1739693128204 in which INA826 is used in unity gain configuration(fig.3). I would like to run a differential AC (50/60Hz) and common mode AC noise rejection for this INA stage. Please do suggest steps to be followed in the TINA simulation software. Additionally I would like to add floating input detection feature in this circuit using simple pullup resistor and pulldown resistor to make INA stage output to 10.24V when input is disconnected. Is it write method to use voltage divider circuit on IN+ pin of INA826?
Best Regards,
Swaminath Katte
Hi Swaminath,
For the differential and common-mode noise rejection, you can implement it via adding differential and common mode capacitors or using the existing X2Y capacitor on the reference design. Here are some reference material on the topic:
common mode and differential filter.pdf
What type of sensor are you planning on connecting to the input? The pullup and pulldown resistor could impact the sensor impedance, so I would caution using this method if the sensor has a low impedance. For the INA826, this method would be fine.
Regards,
Ashley
Thank You for valuable your inputs.
The floating input detection is working fine with circuit configuration as shown below.
"common mode and differential filter.pdf " - I think any additional link is missing for this?
I have further queries on this with respect to end use case.
Queries-
Best Regards,
Swaminath Katte
Hi Swaminath,
Thank you for the additional information. Here is the link again - apologies for the broken link: Link
For your queries:
1. You can use an op amp configuration, but the advantage of the INA solution is that it is able to measure the difference in signals rather than the op amp will need to be built out discretely to do the same function. How you have set up the circuit with the pullup resistor for input detection and the INA should be sufficient.
2. It's recommended to use the AGND as the analog input circuitry should all be connected to the same ground to prevent ground issues. It appears that earth ground is located on the digital side and should be kept separated.
3. The INA has inherent EMI protection via the input stage and is comparable to op amp performance. Please see this app note for more information on EMIRR in general: EMI Rejection Ratio of Operational Amplifiers (With OPA333 and OPA333-Q1 as an Example) (Rev. A) This talks about op amps but is still relevant for INAs.
4. You can simulate multiple types of grounds in TINA but there is not a way to simulate how noise would propagate through grounds. How ground bouncing and signals propagate and couple can only be seen via board testing and it is difficult to simulate this.
Please let me know if you have further questions.
Thank you!