Other Parts Discussed in Thread: THS6182
We are using THS6182.
As you can see on the schematic, the THS6182 is powered in +- 12V and Bias2 is always to 3v.
When we put Bias1 to 0v, amplifier is ON, in low bias mode (cf datasheet).
But, when we put Bias1 to 3.2v, the amplifier is still running instead of sleep mode.
In the screenshot below : pink is Vin1 and blue is gate Q3, with THS6182_ON/ = 3.2V
Do you have any idea of what can happened?
Thanks and regards,
Mickael