Hi evry one
Please help me.
I would like to use the vca810, to keep the sound pressure level constant on the micrphone. The problem is that I have to use a +5V single supply, and I do not see on the datasheet of the 810 VAC that it can be used with a single supply, and since this circuit suits me, I want to know if it can operate with a single supply or if somebody know a similar component with 8, 10, 14 or 16 pins.
Thank you for your help