Other Parts Discussed in Thread: OPA251, OPA364
Hello,
For our new product we need to measure inductivity and DC resistance of a fairly fragile device that can only stand 50-70 mV applied across it for a second or so. The input we have is a 12-bit ADC, and the circuit has to be single-supply (5V). Solution we have now is to first, measure DC voltage drop across device, and then measure AC drop at 1 kHz. Here's what I came up with:
This is AC configuration. R2 is there instead of ADC input.
It simulates well but doesn't really work on the bench, peaking quite wildly. This results in major non-linearity and general unpredictability of output. My guess is that op amps don't really like capacitive loading and inductive sources.
Can anyone help either make this usable or offer an alternative path? Thank you very much!
Alexey