Inheriting an existing design that is very high impedance high gain fempto-amp current to voltage converter (5G Ohm feedback resistor and 1M ohm from sensor to the inverting input. I am new to the guard trace concept, so needing a bit of tutorial here... Now, please be gentle...
In the current configuration the non-inverting input is connected to signal ground. So is the "guard" trace. And the sensor and amplifier package is "shielded" to this same "ground". (You can now imagine the noise on ground, plus what I think is the effective loss of the guard trace).
Questions:
1. without lifting the non-inverting input up through a 10K to "ground", is it legal then to simply join signal (DC) ground to the non-inverting input, and also to "guard"?
2. if we are to create an effective guard in the non-inverting transimpedance mode, can a stable-enough bias be had to keep the output at 0 with no signal in?
3. The current design operates the amplifier with the V- connected to DC ground. I suppose this is reasonable...
Reason for these questions: I've yet to test, but reports are that the noise (and leakage) is apparently high enough to make signal differentiation impossible.