Hello.
I want to ask about pin5 and pin6 (BALANCE) of LM6511.
Please show the reference circuit doing offset adjustment with this balance pin.
And please tell connection when I do not use the balance pin.
Connect 5pin and 6pin directly, and do not do wrong movement?
By the way, there are few high-speed comparators in Wide VIN.
Therefore, the customer is going to choose this device.
If there is the device which I can recommend elsewhere, please show it.
Regards.
k.hashimoto.