Hi,
I am testing a fabricated circuit using LM7171 in Howland current source circuit to supply 10mA in frequency range between 10kHz to 500kHz. I find that during operation the IC at the unity gain buffer (U4) is running hot. Is this indicates that the IC not unity gain stable? or any other reasons for the problems? If the device is not unity gain stable any suggestions for other amplifiers which has stable unity gain? Please advice.
Regards