This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using ina 128 as a comperator in my project. I have used the basic connection that showed in datasheet in page 13. The gain resistor is 2k. I have applied the signal to Vin-(pin 2) input and the reference to the Vin+ (pin 3) input. I have noticed that when there is no signal in pin 2 and I have applied 4.2V to the pin 3, I get 940 mV in the other input (pin 2). Why this is happen? Is it normal? I am using this setup in very precision instrument so this make me fear about unexpected results.
Hi fikret ,
The instrumentation amplifier is used to amplify the differential signal at the + and - pins
i.e the output of the INA will be = Gain X ( Vin+ - Vin-)
I would not recommend that part for your application
I believe you are looking for a comperator , for comparing your reference signal at 4.2V
please find the circuit below with LM393 which is a open collector comparator and would be right fit for your application
Hi fikret,
Thats good to hear , yes you can use it as proportional part of PID
I believe you have kept the (Vin -) pin floating , (that is not connected to any source)
The Instrumentation amplifier is not to be configured with any input pins as floating
Hence the 940mV that you get on the (V -) pin doesn't say anything about the stability or accuracy of the INA128