Other Parts Discussed in Thread: OPA177, INA128, PGA281, INA118, PGA280, INA333
Good morning,
I am working with INA 128 for a project and I am actually testing the amplifier responsivity to the signals I will acquire with a temperature sensor.
The temperature sensor is a prototype and it is basically a full Wheatstone bridge and its outputs range is from 700µV to 7mV. To be sure of the INA performances, the amplifier has been tested separately from the sensor. At INA inputs I have applied signals from 100µV to 20mV using a voltage divider, as shown beow.
Looking to the table below, it is clear the gain is not stable.
|
Vin [mV] |
Vout [mV] |
Gain |
|
0.105 |
0.873 |
8.3 |
|
0.201 |
1.877 |
9.3 |
|
0.305 |
2.899 |
9.5 |
|
0.406 |
3.903 |
9.6 |
|
0.506 |
4.886 |
9.6 |
|
0.603 |
5.863 |
9.7 |
|
0.706 |
6.876 |
9.7 |
|
0.805 |
7.841 |
9.7 |
|
0.910 |
8.861 |
9.7 |
|
1.008 |
9.854 |
9.8 |
|
1.506 |
14.75 |
9.8 |
|
2.005 |
19.75 |
9.8 |
|
2.5 |
24.68 |
9.9 |
|
3.001 |
29.64 |
9.9 |
|
3.505 |
34.65 |
9.9 |
|
4.058 |
40.16 |
9.9 |
|
5.008 |
49.55 |
9.9 |
|
6.018 |
59.55 |
9.9 |
|
7.043 |
69.73 |
9.9 |
|
8.071 |
79.88 |
9.9 |
|
9.137 |
90.54 |
9.9 |
|
10.10 |
100.18 |
9.9 |
|
15.057 |
149.25 |
9.9 |
|
20.023 |
198.64 |
9.9 |
I can expect this for the lowest inputs, because I made the amplifier work out of the input range specifications, but I don’t explain the behavior for the higher values.
Then, I tried the following circuit for trimming the output offset voltage.
I can measure a constant gain only adjusting the output values via the potentiometer on pin 3 of OPA177. I was wondering if anyone knows a better and more practical solution to guarantee a constant gain.
Thanks in advance,
Mia