Part Number: INA826
Other Parts Discussed in Thread: REF3318
So I'm debugging a board that uses INA826 to amplify the output of a wheatstone bridge.
I confirmed the differential inputs to be both at about 1.6 Volts (Wheatstone bridge driven by 3.3V LDO MAX6043).
Differential Voltage is between +/- 3 mV.
VREF is set to 1.8V and provided by NCV8114.
The positive supply of INA826 is provided by a LP38963 LDO at 3.3V.
Here you can see how the wheatstone bridge is connected to the amplifier:

The output of the amplifier doesn't however react to changes in differential input as expected.
When differential input is 0, the ouput looks like this:

This looks okay to me, since VREF = 1.8V (see down below).
But when excitation voltage is raised to about 1mV, the output jumps to .2V.
The VREF-Voltage also jumps from 1.8V to 3.3V
These are the only output voltages I can get.
Here is how I connected the NCV8114:

I suspect that something with my reference voltage is not okay.