This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA193 - Maximum ratings

Other Parts Discussed in Thread: INA193

In the Absolute Maximum Ratings for the INA193, the maximum voltage on the Analog Inputs VIN+ and VIN- says -18V to 18V.

But the simplified schematic at the start of the datasheet shows -16V to +80V on the Analogue Inputs:

Is this an error? Can you please confirm the Absolute Maximum Ratings?

Thanks

 --

Justin