Other Parts Discussed in Thread: TL074, OPA827, OPA627
Hello,
How constant is TL074's output resistance? What parameters affect it?
Stephen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Stephen,
The TL074 is an older device and the output impedance wasn't directly specified in the product datasheet. That said, a functional block diagram for the device is provided in Section 8.2 which shows that the device features a classic common emitter output stage. Similar devices, such as the OPA627 and OPA827 feature flat resistive output impedances over frequency. Therefore, I would expect something similar for the TL074. Since there look to be a passive 128Ohm impedance directly in series with the output and also 64Ohm resistances in series with the transistor impedances, I would expect an open-loop output impedance between 160 and 250 Ohms.
Since we don't have any data to back up the claim our recommendation was to use an overly large deviation of -50% so your system is robust even it if changes by much less than that.
I'm sure what you're asking for with all the current limit and extra resistor questions, but I'll add some additional information that may be helpful. When the output is saturated you'll see the 200 Ohms of output impedance that was calculated in the posts you linked to originally.
When the op amp is operating in a linear condition the open-loop gain (Aol) of the amplifier is very large at low frequencies. In a linear operating condition the closed-loop output impedance (Zout) presented to the load will equal the open-loop output impedance (Zo) divided by 1 + Aol*B, where B (Beta) is the feedback factor and Aol*B is the "Loop-Gain". So for frequencies where the loop-gain is large the closed loop output impedance (Zout) will be small. Lets take an example at 10Hz assuming the open-loop output impedance (Zo) is roughly 200 Ohms and the op-amp is configured in a unity-gain configuration so the loop-gain (Aol*B) is equal to Aol. Since Zout = Zo / 1+Aol*B we can solve for the closed-loop output impedance at 10Hz as shown:
Zout = Zo / (1+Aol*B) = 200 / (1 + 200,000V/V) = 999uOhms (9.99E-4 Ohms).
In my circuit, most of the op-amps feeding the ADC are in an inverting configuration.
According to
.
The output impedance in that type of configuration is equal to the Feedback resistor in parallel with the op-amps output resistance. They assume the output resistance is constant.
However, Equation 9.52 in the pdf at
seems to more closely match what you said.
What happens when the when the op-amp's output voltage exceeds the clamping diode voltage?
My circuit will be relying on the op-amp to limit the current through clamping diodes. Also, I would like the current though the clamping diodes not to exceed 100mA.
Stephen
"The TL074 output resistance should stay with 200 ohms, +/-15%"
Ok, that's good.
"The nice thing about the TL074 is that the output resistance is set almost entirely by resistors."
Do you mean internal op-amp resistors?