Other Parts Discussed in Thread: TINA-TI
Referring to the attached simulation, I am using OPA1632 following the output from ADA4841. The output from ADA4841 has output of 2.2Vpp and offset of 1.78V, I am connecting the output to OPA1632 which has Unity gain just to make output from Single ended to Differential. I have given 2.2 Vpp and im getting 1 V on each side so that is fine but i have a requirement that maximum peak on both outputs should not be more than 2.8V but my output at R9 has reached 3.79 as shown in simualtion. Please suggest how can i adjust my output to be within 2.8V peak.