Other Parts Discussed in Thread: OPA2694
We are cascading two identical THS3202 amplifiers (on the same chip) to achieve a 40-dB gain. This setup is shown in Fig. 3 below, with 200-Ohm R_f and 10.5-Ohm R_g.
When we probe the output of the first amplifier, we see the expected signal with ~20mVpp at 50MHz. This is then fed into the (+) input on the second amplifier. While the (-) input of the second amplifier also show the same waveform (suggesting that feedback is working correctly), the output of the second amplifier oscillates wildly to the full rail (+/- 5V) at >100MHz.
Any idea what we can do to solve this issue?